AXIS#.SETUPREQBITS

Description

This parameter returns the bitwise set status of parameters that needs to be set up before the drive can be enabled. The drive can only be enabled when this parameter returns 0.

The following table lists the parameters which require setup for each motor type.

Index Bit Default Value Linear Permanent Magnet Induction Motor V/f Open Loop Induction Motor Closed Loop Interior Permanent Magnet Brush Motor
AXIS#.IL"Instruction list" This is a low-level language and resembles assembly.KP 0 50 [V/A] -
AXIS#.MOTOR.IPEAK 1 2 Arms
AXIS#.MOTOR.ICONT 2 1 Arms
AXIS#.MOTOR.POLES 4 6 -
AXIS#.MOTOR.LQLL 7 17mH - - - -
AXIS#.MOTOR.LDLL 8 17mH - - - -
AXIS#.MOTOR.KE 9 0 - - - -
AXIS#.MOTOR.IMTR 10 100ms - - - -
AXIS#.MOTOR.IMID 11 0 - - - -
AXIS#.MOTOR.VOLTRATED 12 230 Vrmsrms stands for root mean square (also known as the quadratic mean) - - - -
AXIS#.MOTOR.VRATED 13 0 - - - -
AXIS#.MOTOR.LISAT 14 25 x DRIVE.IPEAK - - - -
AXIS#.MOTOR.VRIDK1 15 0 - - - -
AXIS#.MOTOR.VRIDK2 16 0 - - - -
AXIS#.MOTOR.IDMAX 17 0.5 x AXIS#.MOTOR.IPEAK - - - -
AXIS#.IL.KDPRATIO 18 1 - - - -
AXIS#.MOTOR.PITCH 19 32 - - - -
AXIS#.MOTOR.VOLTMAX 20 480 Vrms - - -

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Integer

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Related Topics

AXIS#.SETUPREQLIST, AXIS#.MOTOR.AUTOSET

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen